To adjust the LCD display on a CM9760-KBD Intelligent keyboard

Issue

LCD display on a CM9760-KBD Intelligent keyboard is too bright or dim.

Product Line

Pelco Matrix

Environment

  • CM9760-KBD Intelligent keyboard

Cause

Adjustment required

Resolution

  1. Turn the CM9760 keyboard over.
  2. Move dip switch number 2 to the on position.
  3. Enter the Setup PIN code (1234 is the default).
  4. Using the 3rd blue key under the LCD display select LCD.
  5. Use the up or down fingers to adjust the display.
  6. Select save.
  7. Select the exit door twice.
  8. Move dip switch number 2 to the off position.
  9. Select the exit door.
  10. Log back into the system as normal.