When using the ONVIF application in Sarix cameras version 1.8.2 we cannot set Multicast to 239.0.0.0

Issue

When using the ONVIF application in version 1.8.2 we cannot set Multicast to 239.0.0.0 - will return with 239.*.*.* where the * are the hosts octet.

Product Line

Pelco Cameras

Environment

Sarix cameras version 1.8.2, when setting the multicast in the ONVIF application.

Cause

We interpret this as 239.*.*.* and fill the rest in with the octet from our host address.

Resolution

There is no resolution at this time, this should be resolved in the next firmware release