CALC is not an option in the DDC editor of a 7700 or 7716.

Issue

CALC is not an option in the DDC editor of a 7700 or 7716.

Product Line

TAC I/NET

Environment

  • DDC Editor
  • 7700
  • 7716

Cause

The Calculation module exists only in MR controllers and ASCs.

Resolution

Use the DCU or PCU Calculation editor. Refer to TCON 209 or TCON 237 for more details about Calculations and DDC modules.