Sarix with Surevision range of IR illumination detected.

Issue

What range of IR illumination will the Sarix with Surevision cameras work?

Product Line

Pelco Cameras

Environment

Sarix "LW" series Cameras with Surevision

Cause

IR Range

Resolution

The cameras will work with any IR illumination from 700nm to 1000nm. The spectral response at 950nm
is lower than at 850nm, it will require 3x more power IR illuminator at 950nm than at 850nm.