Can spectra IV be controlled with P protocol at 9600 baud using Dedicated Micros controllers

Issue

There is an issue with Dedicated Micros control at 9600 baud that prevents control with Pelco PTZ (Pan, Tilt, Zoom) cameras.

Product Line

Pelco Cameras

Environment

All Pelco PTZ Cameras
Dedicated Micros

Cause

The problem is an integration issue.

Resolution

Change the baud rate on the controller and PTZ camera to 4800 baud.