Where do I download the Active X plug-in for the Net300/Net350 Encoders

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

If a browser is used to view live video across the network, there is an Active X plug-in to be installed on the local PC.

Product Line

Pelco Transmission & Power

Environment

Net300 Series 
Net350 Series 

MINIMUM PC REQUIREMENTS (AS NEEDED)

  • PC (Pentium 4 microprocessor, 1.6 GHz) with Windows 98/2000/XP operating system ONLY (Does not have support for higher systems)
  • Network card
  • Internet Explorer 6.0 (or higher) or free serial interface and terminal program
  • Screen resolution of 1024 x 768 or higher, 16- or 32-bit pixel color resolution
     
RAM:

256 megabytes

Graphic Card: ATI RADEON 7500 or 8500, Matrox G 550 or Parhelia ™ , or NVIDIA ® GeForce 3 or 4 with direct show-compatible MPEG-4 playback capability
Ethernet Card: 100 Mbit recommended
Sound Card: Required for audio application
Software: DirectX ® 8.1 or 9.0 application programming interface

Cause

Live video viewed over a web browser.

Resolution

To download the Active X plug-in: https://schneider-electric.box.com/s/v9wju4co0t9hsi67jlutx5plrrajn73q