How do I configure events on the DD423?

Issue

The client desires a scheduled preset position or pattern function to be programmed into the unit.

Product Line

Pelco Cameras

Environment

Spectra IV SE – DD427, and DD435 ONLY.

Cause

The DD423 does not support EVENT programming.

Resolution

The dome drive module must be upgraded to a DD427, or a DD435.