Sarix cameras may not always focus on the full range auto focus when done for the first time

Issue

When doing a "full range auto focus" sometimes the sarix camera will not focus properly

Product Line

Pelco Cameras

Environment

When setting up a Sarix camera for " full range auto focus"

Cause

The home position of the camera will sometime be missed if the camera lens was moved by hand something else cause the home position to be lost.

Resolution

Doing a second "full range auto focus" will  allow the camera to find the home position and re-focus properly.