Issue
Controller Error Log shows error code 5128.
Environment
- Error Log
- Error Code
- NetController
- BCX
- ACX
Cause
An Infinity Controller is dropping offline.
Resolution
- Controller error code 5128 (0x00001408) is an indication that the controllers network comm buffer is out of memory.
- Normally the network transceiver will shut down when this happens to protect the controller.
- This is generally an indication that the controllers comm buffer is being overtaxed. This can happen when there is a data storm present on the network.