ISO 9001 and ISO 14001 certificates for Schneider Electric, LLC

Issue

ISO 9001 and ISO 14001 certificates for Schneider Electric, LLC

Product Line

Andover Continuum, TAC I/A Series, Field Devices, SmartStruxure Solution, Other

Environment

Management Certification Certificate for the Design and Manufacture of Building Management System Controllers, Devices and Electronic Systems.

Cause

The ISO 9001 certificate available on Extranet has expired and the ISO 4001 certificate is not available on Extranet.

Resolution

Download the ISO 9001:2008 certificate for Rockford here and download the ISO 14001:2004 certificate here. Both certificates are valid through to 27th July 2015.

Download the ISO 9001:2008 certificate for Boston here.

For ISO9001 and ISO14001 certificates for Schneider Electric Buildings AB, please see: