Issue
Which adaptor should be used when mounting a M3000 actuator on a V321 DN125/150?
Environment
V321
Forta
M3000
M22
M50
Cause
Forta actuators are a direct fit to V321 on all sizes DN100 and smaller unless stated differently in the catalogues/data sheets.
Resolution
The M3000 actuator will not fit on the V321 DN125 and DN150 sized valves due to the different design of the valve body. For DN125/150, actuators M22 and M50 should be used.