How to Export Personnel Photos.

Issue

Photo export

Product Line

Andover Continuum

Environment

CyberStation

Cause

Need to export photos in personnel records.

Resolution

When a personnel record in Continuum has a photo included, the photo can be exported as a JPG file by doing a "Send to Text File" for that record. 

The JPG file will be created with the following naming convention:  NamePhoto.jpg where name is the object name (uiname).   

The JPG file will be created in the same directory as the DMP file. If multiple personnel objects containing photos are dumped out, a JPG for each will be created in the directory of the DMP file.