Issue
Set up a two wire LTS80 Lini-Temp sensor on a 7718 PCU
Environment
- LTS80 Lini-Temp temperature sensor
- 7718 PCU
Cause
Lini-temp is a type of temperature sensor that is compatible with the I/NET product line.
Resolution
- For Fahrenheit:
- m = 0.21978
- b = -459.6
- For Centigrade:
- m = 0.1221
- b = -273.0
- J31 to 15 VDC
- 10k ohm resistor in slot "A"
- Refer to TCON 106: 7718 PCU Installation Guide for details