Unknown Objects errors when trying to download a b3 controller from an AS.

Issue

During a Continuum to SmartStruxure 1.2 conversion, getting Unknown Object errors when trying to download to B3 controllers with SmartStruxure.

Product Line

SmartStruxure Solution

Environment

  • AS
  • b3
  • Unknown Object
  • Error

Cause

Non StruxureWare objects exist in the b3 controller.

Resolution

Set the ACCID of the b3 controller to 0 using a RoamIO.