I/Net Controllers which are supported with StruxureWare Building Operation 1.3.0 and higher

Issue

I/Net Controllers are Supported in the 1.3.x and higher release of Building Operation

Product Line

TAC I/NET, SmartStruxure Solution

Environment

Site running I/Net and StruxureWare Building Operation1.3.x or higher

Cause

Legacy and support for various I/NET controllers

Resolution

The following controllers are supported:
Routers:
NPR 2000
TAC Xenta 527
TAC Xenta 527-NPR

Site Controllers:
7798b I/Site Controller
7798c I/Site Controller
7793 Micro Controller Interface
7728 I/Site I/O Controller
7780 Distributed Lighting Control Unit
7716 PCU
7718 PCU
7756 PCU
7760 UCI (Unitary Controller Interface)
7700 DCU (MIP01)

7797 ICI (All Versions)

SubLAN Controllers:
72xx Unitary Controllers
7760 Unitary Controller Interface (UCI)
DPU 7910a Door Processing Unit
DPU 7920 Door Processing Unit (DPU 48K)
DIU 7930 Digital Input Unit
DIO 7940 Digital Input Output Unit
SCU 1200 Security Control Unit
SCU 1280 Security Control Unit
SCU 1284 Security Control Unit

MR Controllers (all HVAC)
MR-VAV-AX
MR-VAV-X1
MR-VAV-X2
MR88
MR88R
MR160
MR55
MR55X
MR632
MR-AHU
MR-HP