How do I find the UL Listed Certification number for a Pelco product

Issue

 Safety Certification of Pelco products can be found via the certifying agency’s website.

 
 The UL mark on a product means that UL has determined that it met UL’s safety requirements. The UL marks may only be used on or in connection with products certified by UL and under the terms of written agreement with UL. Products are periodically checked by UL at the manufacturing facility to ensure they continue to meet UL requirements.

Pelco products can bear one of several certification marks. Some Pelco OEM products are evaluated by certifying agencies other than UL (for example, TUV and ETL) but the test standards are the same as those used by UL.

 

 

Product Line

Field Devices, Pelco Cameras, Pelco Monitors, Pelco Video Management, Pelco Matrix, Pelco Transmission & Power

Environment

All Pelco product lines that exhibit the UL listing logo.

Cause

The UL listing website is often difficult to navigate for accustomed visitors.

Resolution

The UL Listings can be found at the following web address:

http://database.ul.com

To begin a basic search for any Pelco product, type Pelco in the company name field. A drop down should appear with Pelco as an option. If the a drop down does NOT appear Click on OPTION and search for Pelco there.

 

  • The Search Results display all Pelco products categorized.

 

 

Unfortunately, all categories will have to be browsed if the specifics of the product are not known.  For example the Sarix network camera IXE Series product line can be found within the category: Information Technology Equipment Including Electrical Business Equipment. Page 2. The certification number can be found at the top of the page:  E194658