Set up a two wire LTS80 Lini-Temp sensor on a 7756 PCU on the lower board

Issue

Set up a two wire LTS80 Lini-Temp sensor on a 7756 PCU on the lower board

Product Line

TAC I/NET

Environment

  • LTS80 Lini-Temp temperature sensor
  • 7756 PCU lower board

Cause

Lini-temp is a type of temperature sensor that is compatible with the I/NET product line.

Resolution