Set up a two wire LTS80 Lini-Temp sensor on a UC

Issue

Set up a two wire LTS80 Lini-Temp sensor on a UC

Product Line

TAC I/NET

Environment

  • UC microcontroller
  • LTS80 Lini-Temp sensor

Cause

Conversion coefficients must be set for proper reading of temperatures.

Resolution

For Fahrenheit:

  • M = 0.4235
  • B = 32.0

For Centigrade:

  • M= 0.2353
  • B = 0.0

The white (WHT) wire of the sensor goes to AI-X of the UC input. The orange (ORN) wire goes to +15v of the UC input.

Refer to TCON 069 for details