Issue
Every 6 second there is an error message in the Vista event log from user "system" that "system failed to log in on node TAVISTA".
Environment
Vista 5.x
Cause
The reason for the messages is that GetAlive is activated for Icarus( a program used in Sweden which sends SMS when a alarms comes to Vista).
Resolution
Deactivate "GetAlive" for Icarus.