How long does it take to update the Continuum database.

Issue

During the uprev of Continuum, the database initialization utility takes a while to update the database.

Product Line

Andover Continuum

Environment

CyberStation

SQL

Cause

Many factors will determine how long it will take for the database update process to complete.

These include but are not limited to:

- Size of the database

- Server performance

- Network performance

Resolution

The main factor determining the time it will take to update the database if its size.

as a guideline a 6 GIG database will take about 30 minutes to update.