Will the I/A Series proprietary drivers work on a JACE-600 or JACE-700?

Issue

Will the JACE-600 or JACE-700 work with any of the four I/A Series proprietary drivers (GCM, DMS, ASD, MS)?

Product Line

TAC I/A Series

Environment

Niagara G3

JACE-600

JACE-700

Cause

Existing building retrofit

Resolution

The four proprietary drivers are not supported on the JACE-600 or JACE-700 controllers. If these drivers are required a JACE 645 (TRD-T-645) is required. Please refer to Product Announcement PA-00251 for further details.