Issue
Each time an InVue graphic screen appears, not all of the dynamic values (tags or remote references) update.
No error messages appear.
Environment
InVue 1.1
WIBS 1.1
Wonderware
Cause
The InVue computer hardware was replaced.
It has a dual/multi-core CPU which was never validated with InVue.
Resolution
Disable the settings in the computer's BIOS such that the CPU behaves like it is a single-core.