Drayton DC1100 / DC1400 controllers - Replacement battery.

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

NOTICE

COMPLEX PROCEDURE REQUIRED.
The resolution of this article has many complex steps that may result in unforeseen results if not performed correctly. If you are at all unfamiliar with the requirements, please contact Product Support Services for assistance.

Issue

Replacement battery for the DC1100 / DC1400.

Product Line

Field Devices

Environment

DC1100

DC1400

Replacement Battery

Cause

Controller battery has failed.

Resolution

The battery lifetime will vary over a very wide range depending on use and temperature so cannot easily be predicted, but about 5 years under normal conditions, would be a guide.

The battery in DC1100 and DC1400 is soldered to the underside of the CPU PCB. It is a 3.6V 150mAh NiMH battery. Our factory part number is S2218121100 and the manufacturer’s part number is Varta 55615 303 059 or 55615 603 940.

 Please Note: - Good soldering skills will be needed to replace the battery. Make sure the person undertaking this knows what they are doing.

They can be bought from Farnell or RS...

To review the Varta 55615 303 059 details at Farnell please click HERE.

To review the Varta 55615 603 940 details at Farnell please click HERE.

To review the Varta 55615 603 940 details at RS please click HERE.