Replacing EM42 actuator on VTRA valve

Issue

EM42 is obsolete and is no longer available when replacement is needed

Product Line

Field Devices

Environment

VTRA linkage kit 8600990000

EM9 180° 8601110000

VTRA valve

EM42

Cause

Replacement of obsolete actuator on old style valve

Resolution

The replacement actuator for EM42 on a VTRA valve is  EM9 180°, 8601110000, together with linkage kit 8600990000. The linkage kit originally included with the EM9 package should NOT be used.