TICC-3/4IN accessory part for Sarix TI Series Fixed Thermal IP Cameras cable entry.

Issue

RG59 coaxial cable will not feed through the adjustable 0.5-inch NPT liquid-tight glands of the Sarix TI Series Fixed Thermal IP Cameras.

Product Line

Pelco Cameras

Environment

  • TI206 Series
  • TI314, TI335, TI350, TI3100 Series
  • TI614, TI635, TI650, TI6100 Series

Cause

The Sarix TI Series 3/4-inch conduit cable cover is designed for use with Sarix TI Series fixed cameras in installations that require the use of 3/4-inch conduit when wiring the camera.

Resolution

Order part# TICC-3/4IN

Install Manual