NOTICE
DISCONTINUED PELCO PRODUCT.This product has been discontinued. For further information please visit pelco.com/support/discontinued-products
Issue
Unable to view live or recorded video for cameras connected to a specific capture card.
Windows Event Viewer error ID 7030 "warning - Board x init error x" (error starts at Board 0 so failure with Board 3 is actually BRD4 in DS Admin) :
Product Line
Pelco Video Management
Environment
DS XPress
Digital Sentry
TX-400
Cause
Hardware failure of the TX-400 capture card.
Resolution
The replacement part number for the TX-400 capture card for DS XPress units: 4601-20003, is no longer available through Pelco.
Contact Pelco for repair or DVR replacement options at 1-800-289-9100.