How to connect audio to an IM10C10 Sarix camera

Issue

Audio with IM10C10 series Sarix cameras.

Product Line

Pelco Cameras

Environment

Specifically, an IM10C10 model Sarix camera, with version 1.7.41 firmware and 2011 or newer hardware, with either a Louroe or Line-In level audio source.

Cause

This article is specific to the IM10C10 model Sarix cameras as no other model of Sarix camera applies.

Resolution

Click the image below to view a larger version in a new window: