How to Factory Reset the Camclosure 2 SD5 Super Dynamic 5 WDR camera?

Issue

Factory Reset steps

Product Line

Pelco Cameras

Environment

IS50/51 Series Camclosure 2 Super Dynamic WDR

Cause

Reset of Camclosure 2 performed to default camera settings

Resolution

To RESET camera:

  1. Hold down the following function keys at the same time: (RIGHT/FAR) + (LEFT/NEAR) + (MENU/SET/ABF2) button for 2 seconds.
  2. Camera flashes the text "REPOR TUDO" once and then goes blank for less that 2 seconds.
  3. Camera will power on and then display serial number.
  4. Camera has been successfully factory defaulted.

See image below for button location