What are the part numbers of the O rings provided in the pressurized Spectra III or Spectra IV?

Issue

Part numbers of O rings provided in the pressurized Spectra III or Spectra IV housing.

Product Line

Pelco Cameras

Environment

Pressurized Spectra III (all models)

Pressurized Spectra IV (all models)

Cause

O ring replacement parts for Pressurized Spectra III or Spectra IV

Resolution

The Spectra Pressurized Series consists of 3 O-rings. Two of the O-rings are factory installed and assembled within the Back Box and the Lower Dome. One O-ring is within the kit bag with O-ring lubricant.

Part numbers and locations of O-rings:

  1. ZH69-0205-2707    O-ring provided for Lower Dome seal.
    MS03-0101-0550    Lubricant tube for O-ring. View installation image here.
     
  2. ZH69-0205-2607    O-ring factory installed for seal of Bubble to Lower Dome. 
                                                                             View factory installation here.
     
  3.  ZH69-0204-1617   O-ring factory installed for seal of Back Box.
                                                                             View factory installation here.


Note: Part numbers are subject to change without notification.

 

Additional lower dome parts that work with All Spectra IV Pressurized analog and IP versions