Pelco protocols supported by the CM6800 and CM6700 Series matrix switch systems.

Issue

What are the programming options for Pelco Protocols of the CM6800, CM6700 Matrix

Product Line

Pelco Matrix

Environment

  • CM6700 - All Models
  • CM6800 - All Models

Cause

Installation and Servicing

Resolution

The CM6700, and CM6800 series matrix switchers support both Pelco D and Pelco P protocols. Additionally, they support Pelco's Standard and Extended Coaxitron protocol.