Part number for tool to open the HS8080 or HS8134 High Security Enclosure

Issue

Key required to open HS8080/HS8134 Enclosure

Product Line

Pelco Cameras

Environment

  • HS8080
  • HS8134

Cause

Key required to perform service on the HS8080 or HS8134 enclosure.

Resolution

 Part number for Tamper Resistant 5/32 key is ZTHEXKEY5/32
 

NOTE: Some earlier models of the HS8080 require the ZTSOCKET10 to remove the security bit.