Add entries in the host’s routing table

Issue

How to add entries in the host’s routing table

Product Line

TAC I/NET

Environment

Command Prompt

Cause

Routing Table Errors

Resolution

As an example: add the address 157.0.0.0

  1. Go to a DOS screen and type the following:
    Route add 157.0.0.0
  2. Then type:
    Route Print
  3. This address should appear.