Site has a I/NET 2000 PCU set as an 06 TAP for ADAA, and the PCU has a synchronous EPROM and synchronous BIN file loaded. Do they need to change the EPROM and BIN file to Asynchronous if they install an integrated dial modem on the serial port of the same PCU?

Issue

Site has a I/NET 2000 PCU set as an 06 TAP for ADAA, and the PCU has a synchronous EPROM and synchronous BIN file loaded. Do they need to change the EPROM and BIN file to Asynchronous if they install an integrated dial modem on the serial port of the same PCU?

Product Line

TAC I/NET

Environment

I/NET site

Cause

Site has a I/NET 2000 PCU set as an 06 TAP for ADAA, and the PCU has a synchronous EPROM and synchronous BIN file loaded. Do they need to change the EPROM and BIN file to Asynchronous if they install an integrated dial modem on the serial port of the same PCU?

Resolution

No, but you do need to use the correct modem, cables, settings, profiles, etc.