How to determine a controller's configuration options.

Issue

Knowing just the serial number of a controller, how to determine the options configured.

Product Line

Andover Continuum

Environment

CX, bcx

Cause

How to determine a controller's configured options when only knowing the serial number.

Resolution

When a controller is online with CyberStation simply run ContinuumExplorer, navigate to the controller, select and right-click on the controller and select Edit. Look at the Options tab.

However, if the controller is non-functioning then contact the US Repair Dept at (978) 475-9600 Press 2 then 3 or via email at tacus.WLCrepair@schneider-electric and provide them with the serial number and controller type. They can look up the options that have been configured.