Issue
After installing Continuum, on launching Cyberstation Continuum does not display the logon dialogue box.
Cannot launch the logon dialogue manually because no Continuum icon appears in the notification area of Windows task bar.
Environment
- Cyberstation
- Continuum
- Logon
Cause
Problem with the OS installation or the corporate image that was used to install the operating system.
Resolution
Following a reformat of the workstations hard drive and reinstallation of the operating system, Cyberstation installed properly.