Replacement for the obsolete TA224 controllers

Issue

Since the TA224 controllers are obsolete, a replacement is requested

Product Line

Field Devices

Environment

TA224V 2241030000

TA224VL 2241040000

Cause

No current products are listed as replacements for the obsolete TA224 controllers.

Resolution

No direct replacements are available- Free programmable Xenta controllers would probably be the only way to replace these old style controllers