Issue
Since all actuators listed in the V392 documentation are obsolete, a replacement is requested.
Environment
- Valve V392
- M5C
- M15C
- EM5C
- M44
- M42
- EM42
- TAC Forta
Cause
Obsolete actuators need to be replaced
Resolution
The Forta series actuators are suitable as replacements. Make sure the correct size is chosen for the application.