What is the minimum pulse duration for the digital inputs (X1 - X3) on a X121-FC?

Issue

What is the minimum pulse duration for the digital inputs (X1 - X3) on a X121-FC?

Product Line

TAC Vista

Environment

TAC Vista 5.1.X

Xenta 121-FC

Cause

The device requires a certain pulse duration to be able to register the feedback signal from another device, such as a fan running signal.

Resolution

The minimum pulse input duration is 250ms.

Click here to open the datasheet for Xenta 121-FC