Where can I download the latest version of DS ControlPoint client software?

Issue

DS ControlPoint client software download location.

Product Line

Pelco Video Management

Environment

  • DS ControlPoint software
    Compatible with:
    • DS series
    • The following DVR's are supported with DS ControlPoint v7.12 and below only, versions 7.13 and greater no longer offer DX support.
      • DX8000/DX8100 series
      • DX4700/DX4800 nonHD series
      • DX4700/DX4800HD series
      • DX4500/DX4600 series
      • DX4100 series

Cause

Latest version DS ControlPoint client software download location.

Resolution

Using the Website (www.pelco.com):

  • Click HERE to access the Digital Sentry page with the download already sorted for Software, scroll down and look for DS ControlPoint Software v.zip file which is most recent version (e.g . DS ControlPointSoftware v7.12.zip). Once located, click the Download link to begin the downloading the software. Make sure to save the file to the local PC, fully unzip the folder before starting the installation.

    Note: When used to connect to a Digital Sentry recorder, it is recommended to download and install the version which matches the Digital Sentry server software version.  The server software version can be found by checking the DS Video Server version in Programs and Features on the recorder.
     

For installation instructions, refer to article: How to install the DS ControlPoint client software.


Related Articles:
How to upgrade the Digital Sentry Software Suite on DSSRV / DSSRV2 / DS NVs HVR(s) and NVR(s).