C20-DW video output level is 1.1v to 1.2v.

Issue

C20-DW over 3rd party UTP modules may display dim or distorted video.

Product Line

Pelco Cameras, Pelco Transmission & Power

Environment

  • C20-DW Series
  • UTP product

Cause

Video output level of C20-DW camera may range from 1.1v to 1.2v.

Resolution

When using C20-DW with 3rd party UTP product, this may require inserting a 120 Ohm resistor at the camera's output or at the end of the cable run.