Meter monitoring in Menta: Menta Macro

Issue

Need Menta programming that can be used to monitor a pulse signal coming from a water meter, electric meter, or gas meter.

Product Line

TAC Vista

Environment

  • Menta
  • Vista

Cause

A Menta program that can be used to monitor water, electric, or gas metering.

Resolution

The program below is set up to receive a pulse signal for three different meters. Click the picture of the Menta macro below to download the source file.