Issue
Can't get the net.x automation KNX OPC server to work with Vista on Win Server 2008 R2
Environment
Win Server 2008 R2
TAC Vista 5.1.X
Cause
A non-compatible version of NetX's OPC server is being used.
Resolution
Use the netX automation Voyager Server UD (Unified Driver) software. This is supported on 64-bit operating systems.