Install CM9760-KBD to a SERCOM port on the CC1

Issue

How do connect a CM9760-KBD keyboard to a SERCOM port on the CM9700-CC1

Product Line

Pelco Matrix

Environment

CM9760-KBD
CM9700-CC1

Cause

Require full-function desktop keyboard that allows to control matrix systems.

Resolution

  1. Make sure all DIP switches are OFF.
  2. Connect the RJ-45 straight cable from the COM 1 port on the keyboard to the "Keyboard" connector on the power supply.
  3. Connect the RJ-45 reversed cable from the "System" connector on the power supply to a SERCOM port on the CC1.
  4. Plug in the power supply.
  5. Turn the main power supply switch ON.

See figure below for connections