How to access the Program Menu of a PTZ Camera sending the Preset 95 Command.

Issue

  • Why can't I call up the Spectra main menu on the monitor with Preset 95?
  • Access Spectra main menu (Preset 95)
  • What is the enter key when navigating the Preset 95 menu?

Product Line

Pelco Cameras, Pelco Video Management, Pelco Matrix

Environment

  • Spectra Series
    • IV, III, Mini
  • CM6700/CM6800
  • KBD200A/KBD300A (Direct Mode Only)
  • KBD300A Connected to CM9700 Matrix System
  • CM9500
  • CM9760-KBD connected to CM9740/CM9760/CM9770/CM9780 Matrix System
  • KBD4000/KBD4002
  • MPT9500
  • NET300/NET350/NET4001A
  • Endura VMS
  • DX Series
    • DX8100/DX8000, DX4700/DX4800, DX4600/DX4500

Cause

Programming preset 95 varies according to the type of controller.

Resolution

Below are instructions for programming preset 95 for various Pelco controllers.

Control in the preset 95 menu

  1. Use the joystick to position the cursor beside the menu selection
    NOTE: If your controller does not have a joystick, use the up or down key
  2. Press Iris Open, the submenu/cursor moves to the right
  3. Move the joystick up or down to view the selections
  4. Press Iris Open to enter the selection.
  5. Press Iris Close to cancel the selection.
     

CM6700/CM6800

  1. Enter the number of the Spectra IV/Spectra IV SE dome system and press the CAM key.
  2. Enter 95 and hold the PRESET key for two seconds.
  3. In the Edit Preset menu, go to SET and press the ACK key. The main menu appears.

KBD200A/KBD300A (Direct Mode Only)

  1. Enter 95
  2. Hold the PRESET key (approximately five seconds) until the main menu appears on the screen.
     

KBD200A/KBD300A

  1. Enter the number of the Spectra IV/Spectra IV SE dome system and press the CAM key.
  2. Enter 95 and hold the PRESET key for two seconds.
  3. Use the KBD200/300A to navigate to SET when connected to a Matrix.
  4. Press the ACK key. The main menu appears.

CM9500

  1. Enter the number of the Spectra IV/Spectra IV SE dome system and press the CAM key. The main menu appears.
  2. Highlight SETUP in the main menu and press the SELECT key.
  3. Highlight CAM in the Setup menu and press the SELECT key.
  4. Highlight PRESET in the Camera menu and press the SELECT key.
  5. Enter 95 and press the F1 key. The main menu appears.

CM9760-KBD Connected to a CM9740/CM9760/CM9770/CM9780 Matrix System

  1. Enter the number of the camera then press the CAM button
  2. Move the joystick to the right and verify that the camera pans right.
  3. Press the ESC key once then press the blue button below the DEF icon. The Define submenu appears.
  4. Enter your four-digit PIN if this is your first time entering this mode use default pin 1234
  5. Press the blue button below the PRST icon
  6. Enter 95
  7. Again, press the blue button below the PRST icon
  8. The main menu appears on the monitor.  Navigate the menus using the joystick.  Use the IRIS OPEN button to select an option
  9. Navigate the menu and select Exit when finished

KBD4000/KBD4002

  1. Press the SPOT MONITOR key.
  2. Enter 95, then hold the PRESET key (approximately five seconds) until the main menu appears on the screen.

MPT9500
Standard Coaxitron Mode

  1. Enter 95 and press the PRESET SET key.
  2. Position the asterisk in the YES row and press the F1 key. The main menu appears.

Extended Coaxitron or RS-485 Mode

  1. Enter 95 and press the PRESET SET key.
  2. Press the F2 key. The main menu appears.

NET300/NET350/NET4001A

  1. Check the Set box.
  2. Click 95 then the preset button. The camera menu appears.

Endura Workstation

  1. Right-click in the video pane of the Spectra IV/Spectra IV SE dome system.
  2. Click Preset and then click Select Preset.
  3. Enter 95 and then click OK.

VCD5000

  1. Enter 95 for the preset action. The shortcuts menu appears.
  2. Press the Preset button on the KBD5000.
     

 DX4000 Series DVR Front panel

  1. Select a channel that is displaying Esprit and Spectra camera, and then press the PTZ/Focus button on the front panel of the DX4000 or on the remote control until the PTZ/Focus controls appear in the lower-right corner of the screen.
  2. Press the up or down arrow button until you have selected preset 95.
  3. Press the channel button numbered 1 (F1 on the remote control). The camera menu appears on the screen.
  4. Navigate through the menu as follows: Press the PTZ/Focus button on the front panel of the DX4000 until the PTZ controls are displayed, and then press the up or down arrow buttons to navigate the list of options.
    Press the PTZ/Focus button on the front panel of the DX4000 until the Focus/Iris controls are displayed, and then press the left arrow button to select an option, or press the right arrow button to deselect an option.
  5. Press the Return button until all menus or commands have been cleared from the monitor.

 

DX4500/4600/4700/4800

  1. Select a channel that is displaying a Pelco PTZ camera
  2. Press the PTZ button on the front panel, the remote control, or the PTZ icon DX4700/4800 PTZ icon the software until the PTZ/Focus controls appear in the right side of the screen
  3. With a mouse select the PGM button to access the menu
    • With the remote:
      • Select SET
      • then select 95
      • then select PRESET
  4. Navigate through the menu as follows:
    • Press up/down arrows to navigate the menu
    • Press the "IRIS +"  button to select and "IRIS -" to cancel


Related Links: