Can ClimateMaster Controllers be integrated with StruxureWare Building Operation?

Issue

ClimateMaster controllers are an OEM version(s) of the I/A MNL LON controllers and can only be added as third party devices in SmartStruxure.  

Product Line

SmartStruxure Solution

Environment

ClimateMaster controllers

SmartStruxure

Cause

ClimateMaster is a channel locked product and will not permit  WorkPlaceTech or WorkPlace Tech Editor to have access to the application via upload or download.

Resolution

ClimateMaster controllers can only be added as third party devices. For help on adding third party devices consult the StruxureWare Building Operation Web Help.

There are three web help topics on adding third party devices:

  • Enterprise Server
  • Automation Server
  • Third-Party Licenses