Cannot add the HistoryPointList object to an ENC Niagara G3 station.

Issue

 The Platform Software Manager shows that the History module is installed in the ENC, but a HistoryPointList object cannot be added to the ENC. 

 The error message “drop failed: java.baja error” is displayed in the Program Director window.

Product Line

TAC I/A Series

Environment

Niagara G3 all version, ENC-410, ENC-520

Cause

The HistoryPointList object requires that the ENC’s Module Content Filter be set to  ui+runtime.

Resolution

Set the ENC’s Module Content Filter Level to ui+runtime.

1. Open the ENC’s Platform and click on Set Module Filter

2. Select ui+runtime and then click on Finish.

The HistoryPointList object can now be added to the ENC.