Issue
Unable to perform a backup or copy files from an I/A Series G3 station - indicates: Error parsing list of remote modules.
javax.baja.sys.LocalizableRuntimeException: Error parsing list of remote modules
Environment
I/A Series G3 (all versions)
Cause
The backup and copy processes include a scan of the remote station's module directory. The software is encountering a file that is not a module and does not have the .jar extension. A user may have transferred a non-module into the directory by mistake.
Resolution
Locate and remove the file causing the issue.
- Using Workbench, connect to the platform of the ENC, JACE, or remote station and run the File Transfer Client.
- Navigate to the /niagara/modules directory that will list out the modules (jar files) installed in the station.
- Review the list to locate the file that is not a module (jar extension).
- Highlight and delete the file.