Improper object references appearing in Occupancy Point field of Infinity Schedule object in Continuum 1.74.

Issue

An Infinity Program object appears In the Occupancy Point field of the schedule editor.

When an attempt is made to browse, select apply the proper occupancy numeric, the same Infinity Program object reference reappears.

Product Line

Andover Continuum

Environment

  • Continuum 1.74
  • Schedules
  • Occupancy Point
  • Database

Cause

This behavior was related to the behavior described in TPA-BOST-08-0005.00

Resolution

This behavior was related to the behavior described in TPA-BOST-08-0005.00