Can the Continuum OPC Server be configured to run as a service?

Issue

Can the Continuum OPC Server be configured to run as a service to enable the application to start without a user having to log on to the relevant machine?

Product Line

Andover Continuum

Environment

Continuum OPC Server

Cause

Need to have OPC Server running without requiring a user to logon to Windows to start the application.

Resolution

No the OPC Server can not be run as a service. It can only be run as an application which will require a user to logon to Windows and start the application.

 

See Lessons Learned Article #5456 for further information on OPC Server.