Priority not changeable message when binding SNVTs

Issue

"Priority not changeable" when binding SNVTs

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation 1.2

Cause

In the XIF file, you can specify if the variable should be sent by default with priority. You can also specify if this should be changeable. If both devices are set to not changeable and they use a different flag in the priority setting, you get this message.

Resolution

The 2 devices are not compatible. You can not make the binding.